Order Statuses

IN PROCESS
Meaning The Order has been started, but has not been submitted
When-Set When an Order is created from a Price and Availability inquiry, Quote or directly
Comments None
PENDING REVIEW
Meaning The agent has requested Cooper to approve the Order in some way. Cooper now has update rights.
When-Set When the user selects the Request Review button
Comments The status will be returned to 'In Process' when Cooper returns the Order to the agent.
SUBMITTED-APPROVED
Meaning An agent has submitted an Order to SAP
When-Set When the user selects the Submit Order button
Comments Only available for Cooper Orders. No outstanding approvals are required. Orders in this status cannot be changed.
SUBMITTED-PENDING
Meaning An agent has submitted an Order to SAP
When-Set When the user selects the Submit Order button
Comments Only available for Cooper Orders. There is usually an outstanding price approval required or a territory split is necessary
CANCELLED
Meaning After issuing a purchase Order, the customer has cancelled the Order.
When-Set When user selects Cancel Order button
Comments The order must be in an In Process' status in order to cancel it. Once the status is set to 'Cancelled', it cannot be changed
SUBMITTED-CHANGE STARTED
Meaning The user begins making changes to an Order that has previously been accepted in SAP
When-Set When the user selects the Change Order button, or chooses the option from the Edit menu of the Order
Comments The Order must be in Submitted-Accepted status before the Change Order option is available.
SUBMITTED-CHANGE PENDING REVIEW
Meaning The user has requested approval for a change made to an Order
When-Set The user chooses to 'Request Change' for the Order
Comments Cooper will grant or deny items where approval is required
SUBMITTED-CHANGE PENDING REVIEW
Meaning The user has requested approval for a change made to an Order
When-Set The user chooses to Request Change for the Order
Comments Cooper will grant or deny items where approval is required
SUBMITTED-CHANGE REQUESTED
Meaning The user has requested a change be made to an Order
When-Set The user chooses to Request Change for the Order
Comments If the changes can be made, Cooper will review the Order and enter the requested information in SAP
SUBMITTED-ACCEPTED
Meaning An Order that was submitted has been accepted in SAP. All Cooper Order Numbers and Line Numbers have returned to FLASH
When-Set When Order Acknowledgement is received from SAP
Comments Once the Order is in this status, it cannot be changed unless the user creates a Change Order. This status comes after Submitted-Approved.
SUBMITTED-CHANGE CANCELLED
Meaning The Order has been cancelled through the Change Order process
When-Set The user selects the Change Order button and then chooses the Cancel Order option from the Edit menu. The user then confirms the cancellation.
Comments The Order is pending Cooper's cancellation approval. Cooper will cancel Order in SAP, if possible.
SUBMITTED-CHANGE REVIEWED
Meaning Cooper Lighting has reviewed a Change Order
When-Set Cooper has returned the Change Order to the Agent user.
Comments The Order is pending Cooper's cancellation approval. Cooper will cancel Order in SAP, if possibleCooper will have already entered the changes in SAP, if the Changes were approved
Back to the top