Who Can Use Flash?

You use Flash either as internal user (i.e. as a Product/Pricing Analyst or as a part of the sales team for Cooper) or an agent - and, of course, each would have their own user setup. The environments for both users are similar for the most part, but there are functions that are available to an agent but not to the internal user and vice versa.

The login page for both looks the same, though! So, you don't need to worry about which environment you're logging into - just type in your username and password.

Headsup!

Since Flash is a client/server application, it needs to be installed on your PC; it cannot be used on the web browser.

To install FlashPro and get your login credentials, you may reach out to the CLSDigitalSupport team: clsdigitalsupport@cooperlighting.com.

Once You have Logged In

The first thing you're going to see when you login is the Homepage, which looks like this:

You will have all the Projects, Quotes and Orders listed out, and you can use this page to open them up. And do you see those little P, Q, O icons at the top, above the list of Projects? That's where you go to open a new Sales Instrument

Note:

Sales Instrument is a catch-all term to indicate project, quotes, and orders. From this point, Project, Quotes and Orders may be referred to as Sales Instrument or SI.

A Tip:

P/Q/O table is displays the most recent SI a user has accessed. This is for convenience only and can be adjusted from 0 to 15 in the User Preferences.

Before we move onto the creation of projects, quotes, and orders, let's get familiarized with Sales Instrument layout.

For the most part, the layout, and the functionalities of the three Sales Instruments are very similar. But much like the difference between an agent login and an internal login, there are certain functionalities that maybe in one SI but not in another.

Flash Sales Instrument Layout

A Project, Quote or Order that is created will always have these four tabs: Header, Line Items, Summary and Additional Header. It is probably worth noting that the Header and Line Items tab are going to be in focus for a lot of this documentation - they are currently very hot and happening and we like to be in vogue.

The Summary Tab allows users to quickly locate all Q/O that are linked to the Project (P) (i.e., File Folder). Projects also has the 'Specification' tab. The 'Additional Header' tab will be covered under Order Manufacturers.

The Menu Bar functionality is a familiar format similar to older Windows operating systems such as Windows XP...or Windows Vista...or whatever came in the late 1900s. Each item on the menu bar contains multiple drop down options that are inherent to the subject line.

Short Cut Icons are located below the Menu Bar.

For a list of all the functionalities check out 'Other Functionalities' under 'How To...'

Sales Instrument Number and Status

The sales instrument Status and Number are displayed in the top right corner of the sales instrument panel as shown below.

The unique SI Number is assigned when the SI is created. This number does not change once it is assigned. You can find the various Sales Instrument Status under 'Appendix'.

The Header

This is where we see the information about the sales such as the agent making the sale, the customer to whom they are selling, the expiration date, etc. The layout varies from projects to quotes to order, but, at minimum, they give you the same set of details - specifically, the agent location, contact and the customers.

Required items (fields) are indicated with red asterisk (*). These fields must be completed in order to Save or progress (continue) within the P/Q/O. Additional fields can be populated based on individual requirements or preferences.

Project Header

Quote Header

Order Header

Line Items

The Line items tab is where the user enters the products being sold and the prices at which they're being sold. The line items in the tab are collectively referred to as Bill of Materials (or BOM).

The 'Bill of Materials' contains Qty, Type Marks, Brand, Catalog Number, Unit Price and Commission. Type Marks and Catalog Numbers are common elements found in a Fixture Schedule.

A 'Line Item' is one item in the BOM. It describes the quantity and price at which the product is being sold at. It includes the following elements:

A Key Point:

Every line item in the BOM must have a quantity. Without quantity, you will not see a commission with the unit price.

Summary

A Summary is available for Projects, Quotes and Orders. There are two ways to access this:

From the homepage

To access the Summary from the Homepage, click on the Project/Quote/Order for which you want to get the summary. The Summary appears in the second half of the screen

From inside the Sales Instrument

Open your Project, Quote and Order, and go to the Summary tab.

The summary has the same details and will even look the same regardless of whether you open it from the Homepage or the Sales Instrument. At a minimum, you will see the Project/Quote/Order name, the agent, and its status. You can also see if they have any other Sales Instrument linked to them (Eg, you can see whether the quote has been converted to an order or if an order is linked to Project, etc.)

Project Summary

Quote Summary

Order Summary

Now that you can navigate through the Sales Instruments, you can go click on the respective links to create a project, a quote and an order.

Back to the top